LTE FDD

Preambles PRACH (EUTRA/eMTC)

For Waveform Playback (ARB) capability.

This topic describes the settings of the Preambles node.

Preamble Assignment

Add Preamble

Delete Preamble

Number of Preambles

Preamble x Settings

Enabled

Power

Resource Block Offset

Preamble Format

Frame Number

Subframe Number

Logical Root Sequence Index

Logical Root Sequence Index (Incremented)

Cyclic Shift Set (High-speed-flat)

Ncs Configuration

Ncs Value

Preamble Index

Physical Root Sequence Index

Cyclic Shift v

Preamble Time Offset

Preamble Configuration Tools

Column Preset

Preset Value

Preset Setting Name

Preamble Assignment

GUI image of Preamble assignment buttons:

Add Preamble

Adds a Preamble to the specified Preamble number. The command argument specifies the position to add a Preamble.

The button is shown in Vertical tab at the same layer of Preamble x.

SCPI Command

[:SOURce]:RADio:LTEFdd:WAVeform[:ARB]:CCARrier<carrier>:PRACh:PREamble:ADD <integer>

SCPI Example

:RAD:LTEF:WAV:CCAR:PRAC:PRE:ADD 7

Notes

Set only (Momentary action)

Preset

–

Min

1

Initial S/W Revision

A.14.00

Delete Preamble

Deletes the specified Preamble.

Button on GUI is indicated in Vertical tab, same layer of Preamble x.

SCPI Command

[:SOURce]:RADio:LTEFdd:WAVeform[:ARB]:CCARrier<carrier>:PRACh:PREamble:DELete <integer>

SCPI Example

:RAD:LTEF:WAV:CCAR:PRAC:PRE:DEL 2

Notes

Set only (Momentary action)

Preset

–

Min

1

Initial S/W Revision

A.14.00

Number of Preambles

This setting is available for SCPI only.

Gets the number of Preambles.

SCPI Command

[:SOURce]:RADio:LTEFdd:WAVeform[:ARB]:CCARrier<carrier>:PRACh:PREamble:COUNt?

SCPI Example

:RAD:LTEF:WAV:CCAR:PRAC:PRE:COUN?

Notes

SCPI only, Query only

State Saved

Yes

Preset

10

Min

0

Initial S/W Revision

A.14.00

Preamble x Settings

Describes the settings of Preamble x, denoting x with preamble number started from 1.

Notes for SCPI:

SCPI mnemonic PREamble<n> denotes PREamble[1]|2|…|<n> where <n> is the configured sequence length.

Enabled

Sets the status of the selected Preamble.

SCPI Command

[:SOURce]:RADio:LTEFdd:WAVeform[:ARB]:CCARrier<carrier>:PRACh:PREamble<n>[:STATe] OFF|ON|0|1

[:SOURce]:RADio:LTEFdd:WAVeform[:ARB]:CCARrier<carrier>:PRACh:PREamble<n>[:STATe]?

SCPI Example

:RAD:LTEF:WAV:CCAR:PRAC:PRE ON

:RAD:LTEF:WAV:CCAR:PRAC:PRE?

State Saved

Yes

Preset

ON

Initial S/W Revision

A.14.00

Power

Enter a power level in dB for the selected Preamble (PRACH burst), relative to the carrier power.

SCPI Command

[:SOURce]:RADio:LTEFdd:WAVeform[:ARB]:CCARrier<carrier>:PRACh:PREamble<n>:POWer <rel_ampl>

[:SOURce]:RADio:LTEFdd:WAVeform[:ARB]:CCARrier<carrier>:PRACh:PREamble<n>:POWer?

SCPI Example

:RAD:LTEF:WAV:CCAR:PRAC:PRE:POW -12.1

:RAD:LTEF:WAV:CCAR:PRAC:PRE:POW?

Notes

Unit in GUI: dB

State Saved

Yes

Preset

0 dB

Min

-60 dB

Max

20 dB

Resolution

0.001 dB

Initial S/W Revision

A.14.00

Resource Block Offset

Sets the number of resource blocks offset for the PRACH preamble.

When the UE Type is set to BL/CE, this value is limited on the narrowbands for each system bandwidth.

{Future} [eMTC] For eMTC PRACH CC, this parameter is initially set to 1 as an exception.

See 3GPP TS 36.211 and 36.331 for more information.

SCPI Command

[:SOURce]:RADio:LTEFdd:WAVeform[:ARB]:CCARrier<carrier>:PRACh:PREamble<n>:RB:OFFSet <integer>

[:SOURce]:RADio:LTEFdd:WAVeform[:ARB]:CCARrier<carrier>:PRACh:PREamble<n>:RB:OFFSet?

SCPI Example

:RAD:LTEF:WAV:CCAR:PRAC:PRE:RB:OFFS 10

:RAD:LTEF:WAV:CCAR:PRAC:PRE:RB:OFFS?

State Saved

Yes

Preset

0

Min

0

Max

44

Max (LP)

Maximum number of RB in the System Bandwidth – 6

Initial S/W Revision

A.14.00

Preamble Format

Sets a value for the PRACH preamble format.

SCPI Command

[:SOURce]:RADio:LTEFdd:WAVeform[:ARB]:CCARrier<carrier>:PRACh:PREamble<n>:FORMat F0|F1|F2|F3

SCPI Example

:RAD:LTEF:WAV:CCAR:PRAC:PRE:FORM F1

:RAD:LTEF:WAV:CCAR:PRAC:PRE:FORM?

State Saved

Yes

Preset

F0

Range

0 | 1 | 2 | 3

Initial S/W Revision

A.14.00

Frame Number

Sets a frame number for the selected PRACH burst.

SCPI Command

[:SOURce]:RADio:LTEFdd:WAVeform[:ARB]:CCARrier<carrier>:PRACh:PREamble<n>:FRAMe <integer>

[:SOURce]:RADio:LTEFdd:WAVeform[:ARB]:CCARrier<carrier>:PRACh:PREamble<n>:FRAMe?

SCPI Example

:RAD:LTEF:WAV:CCAR:PRAC:PRE:FRAM 5

:RAD:LTEF:WAV:CCAR:PRAC:PRE:FRAM?

Notes

Value ranges are determined by the Waveform Generation Length selected in the PRACH Carrier node.

State Saved

Yes

Preset

 

Initial S/W Revision

A.14.00

Subframe Number

Sets a subframe number for the selected PRACH burst.

SCPI Command

[:SOURce]:RADio:LTEFdd:WAVeform[:ARB]:CCARrier<carrier>:PRACh:PREamble<n>:SFRame <integer>

[:SOURce]:RADio:LTEFdd:WAVeform[:ARB]:CCARrier<carrier>:PRACh:PREamble<n>:SFRame?

SCPI Example

:RAD:LTEF:WAV:CCAR:PRAC:PRE:SFR 3

:RAD:LTEF:WAV:CCAR:PRAC:PRE:SFR?

Notes

Value ranges are determined by the Waveform Generation Length selected in the PRACH Carrier node.

State Saved

Yes

Preset

 

Initial S/W Revision

A.14.00

Logical Root Sequence Index

Sets a value for the logical root sequence index.

The Logical Root Sequence Index is the value of RACH_ROOT_SEQUENCE which is the logical index for the Zadoff-Chu sequence used for PRACH preamble generation.

There is the relation between the Logical Root Sequence Index and the Physical Root Sequence Index given by Root Zadoff-Chu sequence order table and preamble format.

See the standard document (3GPP TS 36.211) for more information.

Note) In the case preambles corresponding to Preamble Index cannot be generated from a single root Zadoff-Chu sequence, Logical Root Sequence Index is incremented until corresponding Preamble sequences are found.

That incremented Logical Root Sequence Index is displayed on Logical Root Sequence Index (Incremented) parameter.

Physical Root Sequence Index, Cyclic Shift v and Incremented Logical Root Sequence Index are automatically changed on GUI based on Cyclic Shift Set, Ncs Configuration, Logical Root Sequence Index and Preamble Index.

This parameter is editable only when Configuration Mode is PRACH Configuration.

In the table below, the first Logical root sequence number in the range matches the first Physical root sequence number, the second matches the second, and so on. For example, logical root number 0 = physical root number 129, logical root number 1 = physical root number 710. (See 3GPP TS 36.211.)     

Logical root sequence number

Physical root sequence number µ

(in increasing order of the corresponding logical sequence number)

0 to 23

129, 710, 140, 699, 120, 719, 210, 629, 168, 671, 84, 755, 105, 734, 93, 746, 70, 769, 60, 779, 2, 837, 1, 838

24 to 29

56, 783, 112, 727, 148, 691

30 to 35

80, 759, 42, 797, 40, 799

36 to 41

35, 804, 73, 766, 146, 693

42 to 51

31, 808, 28, 811, 30, 809, 27, 812, 29, 810

52 to 63

24, 815, 48, 791, 68, 771, 74, 765, 178, 661, 136, 703

64 to 75

86, 753, 78, 761, 43, 796, 39, 800, 20, 819, 21, 818

76 to 89

95, 744, 202, 637, 190, 649, 181, 658, 137, 702, 125, 714, 151, 688

90 to 115

217, 622, 128, 711, 142, 697, 122, 717, 203, 636, 118, 721, 110, 729, 89, 750, 103, 736, 61, 778, 55, 784, 15, 824, 14, 825

116 to 135

12, 827, 23, 816, 34, 805, 37, 802, 46, 793, 207, 632, 179, 660, 145, 694, 130, 709, 223, 616

136 to 167

228, 611, 227, 612, 132, 707, 133, 706, 143, 696, 135, 704, 161, 678, 201, 638, 173, 666, 106, 733, 83, 756, 91, 748, 66, 773, 53, 786, 10, 829, 9, 830

168 to 203

7, 832, 8, 831, 16, 823, 47, 792, 64, 775, 57, 782, 104, 735, 101, 738, 108, 731, 208, 631, 184, 655, 197, 642, 191, 648, 121, 718, 141, 698, 149, 690, 216, 623, 218, 621

204 to 263

152, 687, 144, 695, 134, 705, 138, 701, 199, 640, 162, 677, 176, 663, 119, 720, 158, 681, 164, 675, 174, 665, 171, 668, 170, 669, 87, 752, 169, 670, 88, 751, 107, 732, 81, 758, 82, 757, 100, 739, 98, 741, 71, 768, 59, 780, 65, 774, 50, 789, 49, 790, 26, 813, 17, 822, 13, 826, 6, 833

264 to 327

5, 834, 33, 806, 51, 788, 75, 764, 99, 740, 96, 743, 97, 742, 166, 673, 172, 667, 175, 664, 187, 652, 163, 676, 185, 654, 200, 639, 114, 725, 189, 650, 115, 724, 194, 645, 195, 644, 192, 647, 182, 657, 157, 682, 156, 683, 211, 628, 154, 685, 123, 716, 139, 700, 212, 627, 153, 686, 213, 626, 215, 624, 150, 689

328 to 383

225, 614, 224, 615, 221, 618, 220, 619, 127, 712, 147, 692, 124, 715, 193, 646, 205, 634, 206, 633, 116, 723, 160, 679, 186, 653, 167, 672, 79, 760, 85, 754, 77, 762, 92, 747, 58, 781, 62, 777, 69, 770, 54, 785, 36, 803, 32, 807, 25, 814, 18, 821, 11, 828, 4, 835

384 to 455

3, 836, 19, 820, 22, 817, 41, 798, 38, 801, 44, 795, 52, 787, 45, 794, 63, 776, 67, 772, 72, 767, 76, 763, 94, 745, 102, 737, 90, 749, 109, 730, 165, 674, 111, 728, 209, 630, 204, 635, 117, 722, 188, 651, 159, 680, 198, 641, 113, 726, 183, 656, 180, 659, 177, 662, 196, 643, 155, 684, 214, 625, 126, 713, 131, 708, 219, 620, 222, 617, 226, 613

456 to 513

230, 609, 232, 607, 262, 577, 252, 587, 418, 421, 416, 423, 413, 426, 411, 428, 376, 463, 395, 444, 283, 556, 285, 554, 379, 460, 390, 449, 363, 476, 384, 455, 388, 451, 386, 453, 361, 478, 387, 452, 360, 479, 310, 529, 354, 485, 328, 511, 315, 524, 337, 502, 349, 490, 335, 504, 324, 515

514 to 561

323, 516, 320, 519, 334, 505, 359, 480, 295, 544, 385, 454, 292, 547, 291, 548, 381, 458, 399, 440, 380, 459, 397, 442, 369, 470, 377, 462, 410, 429, 407, 432, 281, 558, 414, 425, 247, 592, 277, 562, 271, 568, 272, 567, 264, 575, 259, 580

562 to 629

237, 602, 239, 600, 244, 595, 243, 596, 275, 564, 278, 561, 250, 589, 246, 593, 417, 422, 248, 591, 394, 445, 393, 446, 370, 469, 365, 474, 300, 539, 299, 540, 364, 475, 362, 477, 298, 541, 312, 527, 313, 526, 314, 525, 353, 486, 352, 487, 343, 496, 327, 512, 350, 489, 326, 513, 319, 520, 332, 507, 333, 506, 348, 491, 347, 492, 322, 517

630 to 659

330, 509, 338, 501, 341, 498, 340, 499, 342, 497, 301, 538, 366, 473, 401, 438, 371, 468, 408, 431, 375, 464, 249, 590, 269, 570, 238, 601, 234, 605

660 to 707

257, 582, 273, 566, 255, 584, 254, 585, 245, 594, 251, 588, 412, 427, 372, 467, 282, 557, 403, 436, 396, 443, 392, 447, 391, 448, 382, 457, 389, 450, 294, 545, 297, 542, 311, 528, 344, 495, 345, 494, 318, 521, 331, 508, 325, 514, 321, 518

708 to 729

346, 493, 339, 500, 351, 488, 306, 533, 289, 550, 400, 439, 378, 461, 374, 465, 415, 424, 270, 569, 241, 598

730 to 751

231, 608, 260, 579, 268, 571, 276, 563, 409, 430, 398, 441, 290, 549, 304, 535, 308, 531, 358, 481, 316, 523

752 to 765

293, 546, 288, 551, 284, 555, 368, 471, 253, 586, 256, 583, 263, 576

766 to 777

242, 597, 274, 565, 402, 437, 383, 456, 357, 482, 329, 510

778 to 789

317, 522, 307, 532, 286, 553, 287, 552, 266, 573, 261, 578

790 to 795

236, 603, 303, 536, 356, 483

796 to 803

355, 484, 405, 434, 404, 435, 406, 433

804 to 809

235, 604, 267, 572, 302, 537

810 to 815

309, 530, 265, 574, 233, 606

816 to 819

367, 472, 296, 543

820 to 837

336, 503, 305, 534, 373, 466, 280, 559, 279, 560, 419, 420, 240, 599, 258, 581, 229, 610

SCPI Command

[:SOURce]:RADio:LTEFdd:WAVeform[:ARB]:CCARrier<carrier>:PRACh:PREamble<n>:LRSequence:INDex <integer>

[:SOURce]:RADio:LTEFdd:WAVeform[:ARB]:CCARrier<carrier>:PRACh:PREamble<n>:LRSequence:INDex?

SCPI Example

:RAD:LTEF:WAV:CCAR:PRAC:PRE:LRS:IND 1

:RAD:LTEF:WAV:CCAR:PRAC:PRE:LRS:IND?

State Saved

Yes

Preset

0

Min

0

Max

837 for Format 0 to 3

Initial S/W Revision

A.14.00

Logical Root Sequence Index (Incremented)

Displays a value for the incremented logical root sequence index.

See the standard document (3GPP TS 36.211) for more information.

Note) In the case preambles corresponding to Preamble Index cannot be generated from a single root Zadoff-Chu sequence, Logical Root Sequence Index is incremented until corresponding Preamble sequences are found.

That incremented Logical Root Sequence Index is displayed on Logical Root Sequence Index (Incremented) parameter.

Physical Root Sequence Index, Cyclic Shift v and Incremented Logical Root Sequence Index are automatically changed on GUI based on Cyclic Shift Set, Ncs Configuration, Logical Root Sequence Index and Preamble Index.

SCPI Command

[:SOURce]:RADio:LTEFdd:WAVeform[:ARB]:CCARrier<carrier>:PRACh:PREamble<n>:LRSequence:INDex:INCRemented?

SCPI Example

:RAD:LTEF:WAV:CCAR:PRAC:PRE:LRS:IND:INCR?

Notes

Query only

State Saved

No

Preset

0

Min

0

Max (LP)

837 for Format 0 to 3

Initial S/W Revision

A.14.00

Cyclic Shift Set (High-speed-flat)

Sets the cyclic shift restriction method. The selection of this value is coupled with the value of Ncs Configuration.

Ncs value is determined by Ncs configuration, Cyclic Shift Set and Preamble format.

See the standard document (3GPP TS 36.211) for more information.

Note) In the case preambles corresponding to Preamble Index cannot be generated from a single root Zadoff-Chu sequence, Logical Root Sequence Index is incremented until corresponding Preamble sequences are found.

That incremented Logical Root Sequence Index is displayed on Logical Root Sequence Index (Incremented) parameter.

Physical Root Sequence Index, Cyclic Shift v and Incremented Logical Root Sequence Index are automatically changed on GUI based on Cyclic Shift Set, Ncs Configuration, Logical Root Sequence Index and Preamble Index.

Ncs Configuration

Unrestricted Set Value

Restricted Set Value

0

0

15

1

13

18

2

15

22

3

18

26

4

22

32

5

26

38

6

32

46

7

38

55

8

46

68

9

59

82

10

76

100

11

93

128

12

119

158

13

167

202

14

279

237

15

419

-

SCPI Command

[:SOURce]:RADio:LTEFdd:WAVeform[:ARB]:CCARrier<carrier>:PRACh:PREamble<n>:CSSet RESTricted|UNRestricted

[:SOURce]:RADio:LTEFdd:WAVeform[:ARB]:CCARrier<carrier>:PRACh:PREamble<n>:CSSet?

SCPI Example

:RAD:LTEF:WAV:CCAR:PRAC:PRE:CSS REST

:RAD:LTEF:WAV:CCAR:PRAC:PRE:CSS?

State Saved

Yes

Preset

UNRestricted (Normal Mode)

Range

Unrestricted (Normal Mode) | Restricted (High Speed Mode)

Unrestricted (Normal Mode) (Fixed when PRACH Performance Test for eMTC (36.141) configuration is applied)

Initial S/W Revision

A.14.00

Ncs Configuration

Sets a value for the Ncs configuration.

Ncs value is determined by Ncs configuration, Cyclic Shift Set and Preamble format.

See the standard document (3GPP TS 36.211) for more information.

Note) In the case preambles corresponding to Preamble Index cannot be generated from a single root Zadoff-Chu sequence, Logical Root Sequence Index is incremented until corresponding Preamble sequences are found.

That incremented Logical Root Sequence Index is displayed on Logical Root Sequence Index (Incremented) parameter.

Physical Root Sequence Index, Cyclic Shift v and Incremented Logical Root Sequence Index are automatically changed on GUI based on Cyclic Shift Set, Ncs Configuration, Logical Root Sequence Index and Preamble Index.

NCS  configuration

NCS   value

Unrestricted set

Restricted set

0

0 

15

1

13 

18

2

15 

22

3

18 

26

4

22 

32

5

26 

38

6

32 

46

7

38 

55

8

46 

68

9

59 

82

10

76 

100

11

93 

128

12

119 

158

13

167 

202

14

279 

237

15

419 

-

SCPI Command

[:SOURce]:RADio:LTEFdd:WAVeform[:ARB]:CCARrier<carrier>:PRACh:PREamble<n>:NCS:CONFiguration <integer>

[:SOURce]:RADio:LTEFdd:WAVeform[:ARB]:CCARrier<carrier>:PRACh:PREamble<n>:NCS:CONFiguration?

SCPI Example

:RAD:LTEF:WAV:CCAR:PRAC:PRE:NCS:CONF 10

:RAD:LTEF:WAV:CCAR:PRAC:PRE:NCS:CONF?

State Saved

Yes

Preset

0

Min

0

Max

15 (Unrestricted) for Format 0 to 3

14 (Restricted) for Format 0 to 3

Initial S/W Revision

A.14.00

Ncs Value

Displays the Cyclic Shift value (Ncs value) which is determined by Ncs configuration, Cyclic Shift Set and Preamble format.

See the standard document (3GPP TS 36.211) for more information.

Note) In the case preambles corresponding to Preamble Index cannot be generated from a single root Zadoff-Chu sequence, Logical Root Sequence Index is incremented until corresponding Preamble sequences are found.

That incremented Logical Root Sequence Index is displayed on Logical Root Sequence Index (Incremented) parameter.

Physical Root Sequence Index, Cyclic Shift v and Incremented Logical Root Sequence Index are automatically changed on GUI based on Cyclic Shift Set, Ncs Configuration, Logical Root Sequence Index and Preamble Index.

SCPI Command

[:SOURce]:RADio:LTEFdd:WAVeform[:ARB]:CCARrier<carrier>:PRACh:PREamble<n>:NCS:VALue?

SCPI Example

:RAD:LTEF:WAV:CCAR:PRAC:PRE:NCS:VAL?

Notes

Query only

State Saved

No

Preset

 

Min

 

Max

 

Initial S/W Revision

A.14.00

Preamble Index

Sets a value for the Preamble Index.

The Preamble Index is one of the 64 possible preambles in the cell used for preamble generation.

See the standard document (3GPP TS 36.211) for more information.

Note) In the case preambles corresponding to Preamble Index cannot be generated from a single root Zadoff-Chu sequence, Logical Root Sequence Index is incremented until corresponding Preamble sequences are found.

That incremented Logical Root Sequence Index is displayed on Logical Root Sequence Index (Incremented) parameter.

Physical Root Sequence Index, Cyclic Shift v and Incremented Logical Root Sequence Index are automatically changed on GUI based on Cyclic Shift Set, Ncs Configuration, Logical Root Sequence Index and Preamble Index.

Test preambles for Normal Mode

Burst Format

Ncs value

Logical Root Sequence Index

Cycle Shift v

0

13

22

32

1

167

22

2

2

167

22

0

3

0

22

0

4

10

0

0

Test preambles for High Speed Mode

Burst Format

Ncs value

Logical Root Sequence Index

Cycle Shift v

0

15

384

0

1

202

384

0

2

202

384

0

3

237

384

0

Refer to Preamble Index in TS36.321 5.1, TS36.331 6.3.2, and TS36.212 5.3.3.1.3.

SCPI Command

[:SOURce]:RADio:LTEFdd:WAVeform[:ARB]:CCARrier<carrier>:PRACh:PREamble<n>:PINDex <integer>

[:SOURce]:RADio:LTEFdd:WAVeform[:ARB]:CCARrier<carrier>:PRACh:PREamble<n>:PINDex?

SCPI Example

:RAD:LTEF:WAV:CCAR:PRAC:PRE:PIND 10

:RAD:LTEF:WAV:CCAR:PRAC:PRE:PIND?

State Saved

Yes

Preset

0

Min

0

Max

63

Initial S/W Revision

A.14.00

Physical Root Sequence Index

Displays the physical root sequence index.

There is the relation between the Logical Root Sequence Index and the Physical Root Sequence Index given by Root Zadoff-Chu sequence order table and preamble format.

See the standard document (3GPP TS 36.211) for more information.

Note) In the case preambles corresponding to Preamble Index cannot be generated from a single root Zadoff-Chu sequence, Logical Root Sequence Index is incremented until corresponding Preamble sequences are found.

That incremented Logical Root Sequence Index is displayed on Logical Root Sequence Index (Incremented) parameter.

Physical Root Sequence Index, Cyclic Shift v and Incremented Logical Root Sequence Index are automatically changed on GUI based on Cyclic Shift Set, Ncs Configuration, Logical Root Sequence Index and Preamble Index.

SCPI Command

[:SOURce]:RADio:LTEFdd:WAVeform[:ARB]:CCARrier<carrier>:PRACh:PREamble<n>:PRSequence:INDex?

SCPI Example

:RAD:LTEF:WAV:CCAR:PRAC:PRE:PRS:IND?

Notes

Query only

State Saved

 

Preset

 

Min

 

Max

 

Initial S/W Revision

A.14.00

Cyclic Shift v

Displays the cyclic shift v which is used for cyclic shift calculation of preamble generation.

See the standard document (3GPP TS 36.211) for more information.

Note) In the case preambles corresponding to Preamble Index cannot be generated from a single root Zadoff-Chu sequence, Logical Root Sequence Index is incremented until corresponding Preamble sequences are found.

That incremented Logical Root Sequence Index is displayed on Logical Root Sequence Index (Incremented) parameter.

Physical Root Sequence Index, Cyclic Shift v and Incremented Logical Root Sequence Index are automatically changed on GUI based on Cyclic Shift Set, Ncs Configuration, Logical Root Sequence Index and Preamble Index.

Test preambles for Normal Mode

Burst Format

Ncs

Logical Root Sequence Index

Cycle Shift v

0

13

22

32

1

167

22

2

2

167

22

0

3

0

22

0

4

10

0

0

Test preambles for High Speed Mode

Burst Format

Ncs

Logical Root Sequence Index

Cycle Shift v

0

15

384

0

1

202

384

0

2

202

384

0

3

237

384

0

Refer to Preamble Index-related information in TS36.212 5.3.3.1.3, TS36.321 5.1, and TS36.331 6.3.2.

SCPI Command

[:SOURce]:RADio:LTEFdd:WAVeform[:ARB]:CCARrier<carrier>:PRACh:PREamble<n>:CSHift:V?

SCPI Example

:RAD:LTEF:WAV:CCAR:PRAC:PRE:CSH:V?

Notes

Query only

State Saved

 

Preset

 

Min

 

Max

 

Initial S/W Revision

A.14.00

Preamble Time Offset

Sets the preamble time offset in microseconds (us) for the selected burst.

SCPI Command

[:SOURce]:RADio:LTEFdd:WAVeform[:ARB]:CCARrier<carrier>:PRACh:PREamble<n>:TIMing:OFFSet <numeric>

[:SOURce]:RADio:LTEFdd:WAVeform[:ARB]:CCARrier<carrier>:PRACh:PREamble<n>:TIMing:OFFSet?

SCPI Example

:RAD:LTEF:WAV:CCAR:PRAC:PRE:TIM:OFFS 0.1us

:RAD:LTEF:WAV:CCAR:PRAC:PRE:TIM:OFFS?

Notes

Valid values are as follows:

0.0 us, 0.1 us, 0.2 us, 0.3 us, 0.4 us, 0.5 us, 0.6 us, 0.7 us, 0.8 us, 0.9 us

State Saved

Yes

Preset

0.0 us

Min

0.0 us

Max

0.9 us

Initial S/W Revision

A.14.00

Preamble Configuration Tools

Column Preset

Preset values of parameters for all preambles.

SCPI Command

N/A

Notes

Set only (Immediate Action)

State Saved

No

Preset

Refer to the element definition of the data part below.

Range

Refer to the element definition of the data part below.

Initial S/W Revision

A.14.00

Preset Setting Name

Selects a setting name to preset.

SCPI Command

–

SCPI Example

–

Notes

Set and Query

GUI label: Column

Value selection: Pulldown menu

State Saved

No

Preset

Enabled

Range

Refer to the element definition of the data part below.

Initial S/W Revision

A.14.00

Preset Value

Selects a value to preset for the selected setting.

SCPI Command

–

SCPI Example

–

Notes

Set and Query

GUI label: The name of selected setting in Column

Value selection: Depends on the selected setting. Refer to the section of the selected setting

State Saved

No

Preset

Depends on the selected setting. Refer to the section of the selected setting

Range

Refer to the element definition of the data part below.

Initial S/W Revision

A.14.00

Carrier PRACH ARB

Welcome to LTE FDD